Ingrem Gaming Chair Board Wiring / Photos Needed
Hello everyone,
I’m working on diagnosing and rewiring the control system for an Ingrem Veyron J20 gaming chair. The chair uses a servo module with an RJ45 connection to the handheld remote, and I’ve been tracing signals back to the main board (marked ST‑H801S‑V1.1 and ST‑H8‑CORE‑V2.1).
Here’s what I’ve established so far:
RJ45 pinout from the remote:
Pin 1 → Green (likely RX)
Pin 2 → Black (Ground)
Pin 3 → Yellow (TX??
Pin 4 → White (logic/handshake line, not VCC)
The board itself has a separate AC power feed.
With RJ45 disconnected, the board powers up fine (red LED lights). When RJ45 is wired incorrectly, the board fails to boot.
- I believe the connections come from UART1 and COM20, but I don’t know how they should map to the RJ45 connector
:question_mark:What I Need
If anyone here owns an Ingrem Veyron J20 chair, could you please:
Photograph the main board (ST‑H801S / ST‑H8‑CORE) with the connectors attached.
Show the RJ45 wiring harness and how the colored wires (green, black, yellow, white, red) are mapped.
Confirm whether the white line is actually used for handshake or left floating.
Why This Matters
I’m trying to restore full functionality (servo + remote control). Having a clear photo of the board with connections would save a lot of guesswork and confirm the correct pinout.
Any help, teardown shots, or wiring notes from fellow Ingrem chair owners would be hugely appreciated.
Thanks in advance