Skip to main content
GBobe.1
Visitor II
March 2, 2023
Solved

Is STW13NK100Z available as an SMD?

  • March 2, 2023
  • 1 reply
  • 702 views

trying to avoid through hole part, would prefer a SMD part.

This topic has been closed for replies.
Best answer by Peter BENSCH

Welcome, @GBobe.1​, to the community!

This STW13NK100Z with exactly the same parameters is not available as SMD, but you can look at the STH12N120K5-2, which has a slightly higher Rdson, but can even switch 1200V instead of only 1000V.

The only other alternative in this voltage class would be the same device STH13N120K5-2AG with essentially the same parameters, but with automotive approval.

Does it answer your question?

Regards

/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
March 2, 2023

Welcome, @GBobe.1​, to the community!

This STW13NK100Z with exactly the same parameters is not available as SMD, but you can look at the STH12N120K5-2, which has a slightly higher Rdson, but can even switch 1200V instead of only 1000V.

The only other alternative in this voltage class would be the same device STH13N120K5-2AG with essentially the same parameters, but with automotive approval.

Does it answer your question?

Regards

/Peter