Skip to main content
ZJing.1
Associate
October 31, 2022
Solved

Is there a replacement for the ST10F273MR-4Q3?

  • October 31, 2022
  • 4 replies
  • 1117 views

I have a need for ST10F273MR-4Q3, but this material has been discontinued, is there a replacement for it, preferably in the same package?

This topic has been closed for replies.
Best answer by Peter BENSCH

Well, there are a very large number of potential candidates, but an exact recommendation depends very much on the peripheral units currently in use and your requirements.

If, for example, two CAN MAC are absolutely necessary, the STM32H745ZG comes into question, which otherwise offers considerably more functions and performance than the ST10F273M. It's a bit like comparing a Ford Model T with a Tesla Model Y.

For support with the redesign, I recommend contacting a local distributor.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

4 replies

Peter BENSCH
Technical Moderator
November 1, 2022

Welcome, @ZJing.1​, to the community!

the ST10F273M is unfortunately discontinued without replacement, there is no alternative that can be used because the technology is completely obsolete. The only remaining options:

  • remaining quantities at dealers
  • redesign of the board

I am sorry not to be able to give a more positive answer.

Regards

/Peter

ZJing.1
ZJing.1Author
Associate
November 3, 2022

Thank you for your reply

ZJing.1
ZJing.1Author
Associate
November 3, 2022

If the board is redesigned, what model can functionally replace it?Is there any good advice?

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
November 3, 2022

Well, there are a very large number of potential candidates, but an exact recommendation depends very much on the peripheral units currently in use and your requirements.

If, for example, two CAN MAC are absolutely necessary, the STM32H745ZG comes into question, which otherwise offers considerably more functions and performance than the ST10F273M. It's a bit like comparing a Ford Model T with a Tesla Model Y.

For support with the redesign, I recommend contacting a local distributor.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter