Skip to main content
August 4, 2022
Question

Is there any option to auto update X-NUCLEO-LPM01A Firmware?

  • August 4, 2022
  • 2 replies
  • 1028 views

Hi ST family,

I want X-NUCLEO-LPM01A's firmware to auto upgrade. Is there any way to do or we should have to do manually?:grinning_face:

    This topic has been closed for replies.

    2 replies

    Peter BENSCH
    Technical Moderator
    August 8, 2022

    Welcome, @DJohn.16​, to the community!

    Even though the STM32L496VGT6 included in the kit has a dual bank read-while-write Flash, an auto-upgrade of the firmware would require a special bootloader that supports this and of course a data source including the connection to it from which the upgrade can be obtained. However, the source code for the kit is not available, so you can only upgrade manually.

    Does it answer your question?

    Regards

    /Peter

    November 15, 2022

    Nope, Only manual