Skip to main content
NC.1
Visitor II
May 19, 2021
Question

Issue in reading the EEPROM data via SPI

  • May 19, 2021
  • 1 reply
  • 588 views

Hi,

We are using MPC5xxx uC and configured single SPI channel for 3 different devices.

One of the device is EEPROM (M95256-DRE) and SPI channel is configured as 'Synchronous' mode.

Issue :

Before configuring the SPI channel for EEPROM, the two devices were able to successfully get the transmit / receive the data via SPI channel.

We tried testing the EEPROM independently and we were able to read / write the data from / to EEPROM successfully (Here the other two devices functionality was disabled).

When all the 3 devices functionality is enabled, we observed the below issue :

Scneario 1 : When EEPROM alone is requested to transmit the data we are able to receive the data from EEPROM.

Scneario 2 : Sequentially we are utilizing the SPI channel to get the data from EEPROM and other devices in below mentioned sequence.

Step 1 : Send command to get the data from EEPROM. Here we are getting correct data.

Step 2 : Send command to get the data from other devices. Here we are getting correct data.

Step 3 : Send command to get the data from EEPROM . Here we are getting zero value from EEPROM but the request is transmitted successfully.

From the above observation we have a query that whether EEPROM needs a dedicated SPI channel.

Could you please answer the above mentioned query and help us resolve the above mentioned issue at the earliest.

Thank you.

This topic has been closed for replies.

1 reply

Pierre P.
ST Employee
May 25, 2021

Hello,

Yes i recommend a dedicated SPI channel for the EEPROM. (At least /S line)

Note: Step 3 seems to be corrupted by data transmitting from other devices.

Best Regards

Team EEPROM suPPort