Skip to main content
DRicc.2
Associate III
October 27, 2024
Question

Issue with MCP4541-104E/MS digital pot

  • October 27, 2024
  • 0 replies
  • 796 views

I recently created a digital potentiometer breakout board for the MCP4541-104E/MS, where I would set the resistance value dependent on a particular wiper value. Here is the schematic and layout (I changed the pullups from 10k to 4.7k):

 

DRicc2_0-1730053887909.png

DRicc2_1-1730053911904.png

 

Here is the code:

 

#include "main.h"
#include <stdio.h>
#include <string.h>
#define MCP4541_ADDR 0x2C // Device Address
#define WIPER_CMD 0x00 // Command to set the wiper


I2C_HandleTypeDef hi2c1;

UART_HandleTypeDef huart2;

char msg;

void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
static void MX_USART2_UART_Init(void);

void Set_Potentiometer(uint8_t wiperValue) {
 uint8_t data[2];
 data[0] = WIPER_CMD; // Command
 data[1] = wiperValue; // Wiper value
 HAL_I2C_Master_Transmit(&hi2c1, MCP4541_ADDR << 1, data, 2, HAL_MAX_DELAY);
}

void Print_Value_Uart(uint8_t wiperValue) {
 char msg[50];
 sprintf(msg, "Wiper set to: %d\r\n", wiperValue);
 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
}



int main(void)
{


 HAL_Init();


 SystemClock_Config();


 MX_GPIO_Init();
 MX_I2C1_Init();
 MX_USART2_UART_Init();


 while (1)
 {
	 HAL_Delay(1000);


	 static uint8_t currentWiperValue = 12; // Set to 5kΩ

	 // Set the new wiper value
	 Set_Potentiometer(currentWiperValue);

	 // Print the current wiper value via UART
	 Print_Value_Uart(currentWiperValue);


 }

}

 

 

I am using PB6 as my SCL and PB7 as my SDA on the Nucleo L476RG. I have HVC/AC pulled to ground and wiper pin B pulled to ground. The POW pin is connected to a green LED with a 1k resistor tied to ground. P0A is floating. 

The resistance value across P0A and P0B is 100k and P0A and P0W is 50k, regardless of what I set the wiper value to. I checked the SCL and SDA lines with a scope and I am getting signals sent every second, and the UART terminal outputs the following:

DRicc2_2-1730054219730.png

I'm unsure what is missing in my code or setup, any help would be appreciated.