Associate
February 7, 2020
Question
LDP01-35AY ISO16750-2 pulse
- February 7, 2020
- 4 replies
- 1903 views
Dear sir or madam,
we are using the LDP01-35AY twice in our design for input protection as given in ISO 7637-2 and ISO 16750-2. Unfortunately the load dump pulse destroys our input circuit. I did an extrapolation of the "Safe Operation Mode" of the diode as given in the datasheet page 4. By this I thought the diode is suitable to protect from Load Dump Pulses with 150 V at td = 400 ms and 180 V at td = 150 ms. We tested 150 V with td = 400 ms and the diode immediately was detroyed. Do you have any other parts? Why does the diode get destroyed? We need to be compliant with the ISO 16750-2 therefore 150 V at td = 400 ms is the minimum for us.
Best regards
Marc