Skip to main content
Visitor II
April 4, 2025
Solved

M24512E-F NC pins

  • April 4, 2025
  • 1 reply
  • 259 views

Hi ST Community,
Are the NC pins completely isolated from the device. Wishing to know if there would be a problem with them being driven, pulled to VCC or to VSS.

Thanks!

Best answer by Peter BENSCH

Welcome @M1_it, to the community!

It is not a problem to connect the NC pins to VCC or VSS. This has no effect on functionality or reliability.

Hope that helps?

Regards
/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
April 4, 2025

Welcome @M1_it, to the community!

It is not a problem to connect the NC pins to VCC or VSS. This has no effect on functionality or reliability.

Hope that helps?

Regards
/Peter