Skip to main content
MMici.1
Associate II
September 28, 2025
Solved

M24C04-F DNF5 I2C address

  • September 28, 2025
  • 2 replies
  • 296 views

Dear All,

can someone, please, specify the meaning of the bit 1 as 'A8' in the I2C address of the M24C04-FMH6TG?

MMici1_0-1759081896628.png

I can't find any explanation of this value.

 

Thank you

Best answer by Peter BENSCH

The M24C04 contains 512 (2^9) bytes, which require 9 bits for addressing. Since an address byte only has 8 bits (A0...A7), the 9th bit (A8) must also be transferred, for which bit b1 in the device select code is used.

Does it answer your question?

Regards
/Peter

2 replies

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
September 29, 2025

The M24C04 contains 512 (2^9) bytes, which require 9 bits for addressing. Since an address byte only has 8 bits (A0...A7), the 9th bit (A8) must also be transferred, for which bit b1 in the device select code is used.

Does it answer your question?

Regards
/Peter

MMici.1
MMici.1Author
Associate II
October 1, 2025

Of course, thanks :D.