Associate II
August 20, 2017
Question
parameters of the transformer
- August 20, 2017
- 2 replies
- 1300 views
Posted on August 20, 2017 at 16:20
Hi
my name is pini i work on new project AC/DC converter
the input is 85-265 VAC
output 12vdc/350mA
axiliry :16vdc
chip:viper013HS
I work with a midcom transformer 750370024 and viper013hs
I don't how to set this transformer in simulate (how to enter the parameters)
this is EE13/7/4 but
I do not have all the
parameters of the transformerHow can i run the simulation correctly?
thanks