Skip to main content
Associate
January 22, 2025
Solved

Request for Feedback on Schematic and Queries - ST33TPHF2XI2C

  • January 22, 2025
  • 1 reply
  • 387 views

Hello, 

We are considering using the ST33HTPH2X32AHD5 for our application. This IC has four GPIOs (GPIO_PP, GPIO_LP, GPIO_D, GPIO_C), along with RESET and IRQ pins. We have the following questions regarding these pins:

1) Can you recommend which GPIO pins should be used/connected to the controller?

2) Can the GPIO pins be left open if not in use?

3) Is a 10k pull-up resistor required on the RESET pin?

4) Is a 10k pull-up resistor required on the IRQ pin?

5) We have added a 2k pull-up on the I2C lines. Is a 2k pull-up acceptable for this application?

 

 

6) We have also attached the schematic for your review. 

Please review and provide you feedback and suggestion. 

sonaliz_0-1737536505869.png

 

Thanks,

Sonali

Best answer by Peter BENSCH

The data of all ST33 devices is strictly confidential and will only be handed over if an NDA is signed. For this reason, nobody in the public community will be able to help you, so you should contact your local ST contact.

Hope that helps?

Regards
/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
January 22, 2025

The data of all ST33 devices is strictly confidential and will only be handed over if an NDA is signed. For this reason, nobody in the public community will be able to help you, so you should contact your local ST contact.

Hope that helps?

Regards
/Peter