Skip to main content
pavel2
Visitor II
August 8, 2016
Question

ST1CC40DR too hot on 3A

  • August 8, 2016
  • 1 reply
  • 763 views
Posted on August 08, 2016 at 21:51

Hi! I have made a scheme for CREE X-ML2 LED (with maximum output at 3A) in eDesign studio. But missed that IC loses 0.8w power at 3A and getting very hot quickly, then stepdown output current to ~2A. Is there any way to fix it without total redesign(with different IC) or big additional heatsink on IC?

This topic has been closed for replies.

1 reply

Patrizia BELLITTO
ST Employee
August 24, 2016
Posted on August 24, 2016 at 12:10

Dear sir,

the ST1CC40 is a synchronous step down current source with internal high side and low side switch. The switching frequency is fixed and equal to 850KHz. For these reasons, the power losses of the device are due to the selected application conditions, not to the external components selection.