Skip to main content
AFidi.1
Associate II
February 9, 2023
Question

Teseo-LIV3FL Low Power Mode Not Working

  • February 9, 2023
  • 5 replies
  • 2449 views

I'm using a Teseo-LIV3FL GNSS module for my project and trying to set the low power mode settings using Teseo-Suite software. Tried using the Low Power settings from the wizard but after get the fix it still draws around 50mA of current.

Expected behavior: After getting a fix it'll go to sleep for certain period of time (around 60s and only draws small amount of current) before logging the data again (periodic low power mode I guess (?))

What is the correct way to achieve the expected behavior?

    This topic has been closed for replies.

    5 replies

    ST Employee
    February 9, 2023

    Hello @AFidi.1​ 

    Have you checked the software user manual ?

    AFidi.1
    AFidi.1Author
    Associate II
    February 9, 2023

    Yes I've checked the manual. I also tried sent the command manually but still no luck.

    $PSTMSETPAR,1200,E70000,2
    $PSTMSETPAR,1200,E70000,1
    $PSTMSETPAR,1227,3C0,2
    $PSTMSETPAR,1227,C0,1
    $PSTMSAVEPAR
    $PSTMSRR

    Rebooted di GNSS firmware and still no luck.

    AVike.1
    Visitor II
    February 12, 2023

    Hello, @AFidi.1​ 

    In case if you use an external antenna, Teseo doesn't turns off antenna's power line (X-Nucleo GNSS board with Teseo-liv3f), as I understand. May be it will be usefull to check power consumption without any antenna.

    AVike.1
    Visitor II
    February 12, 2023

    Also, to turn ON the Low power algorithm you need to set-up the 31 bit of CDB-ID 200:

    $PSTMSETPAR,1200,80E70000,2

    AFidi.1
    AFidi.1Author
    Associate II
    February 12, 2023

    Hi,

    Thank you for your response. Anyway, I've tried using $PSTMLOWPOWERONOFF and now its working as expected.

    However, now I got another issue. I'm trying to set geofence using $PSTMGEOFENCECFG and it says $PSTMGEOFENCECFGERROR*06 and here's the command that I sent to my Teseo.

    0693W00000YAX4uQAH.pngDo you know where did I go wrong? I'm kinda lost since it only says error without any details.

    AVike.1
    Visitor II
    February 13, 2023

    May be, ID should start from 1?

    AVike.1
    Visitor II
    February 13, 2023

    And radius value format as double: 1200.0?