Skip to main content
Associate
June 15, 2024
Solved

"The interface firmware FAILED to reset/halt the target MCU" .txt with STEVAL-SPIN3202

  • June 15, 2024
  • 1 reply
  • 2413 views

Hello,

I am working with STEVAL-SPIN3202 to develop motor control solution. I am using the Motor Control Workbench 6.2.1. 

I could generate the project using the workbench, however when i Connect the evaluation board, window with FAIL.txt opens which reads "The interface firmware FAILED to reset/halt the target MCU".

Thus I am not able to connect to the board. I have tried connecting to the board using ST-Link Utility, however it gives the error message "Can not connect to target".

I have tried some of the solution mentioned on the forum but the issue still persist.

Please guide me so that i can get my motor running.

Best answer by AScha.3

To the board...see manual:

AScha3_0-1718441499041.png

 

1 reply

AScha.3
Super User
June 15, 2024

Hi,

ST-Link Utility is old, deprecated. Dont use this .

So try with CubeProgrammer , connect "under reset" or "software reset" .

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
D_AnkitAuthor
Associate
June 15, 2024

Hi,

Thank you for your reply. Tried with CubeProgrammer. Still no luck. It throws below error and when the board is connected FAIL.txt is still generated.ST_error.png

AScha.3
Super User
June 15, 2024

Hi,

"no target found" is just info: cannot connect...

So show, what CubeProgrammer shows...target voltage...etc.

so:

AScha3_0-1718436545102.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."