Question
Unable to setup I2C communication between 2 x STM32F103 blue pill boards.
- January 16, 2026
- 3 replies
- 352 views
Hello,
I am unable to setup I2C communication between 2 x STM32F103 blue pill boards. I have pasted code and the hardware setup below. Would appreciate help trying to pinpoint the problem.
Hardware setup:
- Both boards are connected to an adapter via an ST-LINK V2 with SWCLK, SWDIO, GND, and 3.3V connections.
- SCL pins are connected together (B6 -> B6) and SDA pins are connected together (B7 -> B7)
- The SCL and SDA pins of the Master STM32 are connected to 3.3V via 4.7kΩ resistors.
- The GND of Master and Slave are connected together
- I have probed all the pins and they are at the correct levels so I doubt hardware is the problem (see image attached)
Software setup:
- One thing worth mentioning is that trying to debug the projects through the IDE results in the following message: "Target no device found... Error in initializing ST-LINK device. Reason: No device found on target."
- Therefore I have been running the project on STM32CubeProgrammer using the bin file that gets generated after running the file on the IDE. Also, the only way to connect to the STM is by holding the reset button on the STM, pressing connect, then letting go of the reset button. I wonder if this Temu way of connecting to the STM has anything to do with my shortcomings.
I2C Configuration:
- The GPIO settings for both SDA and SCL have "No pull-up and no pull-down" indicated, the maximum output speed is "Low"
- The clock speed is 100kHz
- The slave has "I2C1 event interrupt" and "I2C error interrupt" enabled but the master does not.
Run Procedure:
- 1. Flash to master
- 2. Take out Master ST-LINK, Flash to slave
- 3. Plug back in the Master ST-Link so they both flash together
- Currently the PC13 LED for Master is off so it is sending the data but the PC13 LED for the slave is stuck at 50ms blink speed so I don't think it is seeing the sent
Firmware setup:
Master:
- Sends a bit stream of all 1's (0xFF) or all 0's to the slave (0x00)
- Turns on an LED if there is an error or NACK:
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_I2C1_Init();
while (1)
{
HAL_StatusTypeDef status;
//send address byte, wait for acknowledge from slave, send 1 data byte
status = HAL_I2C_Master_Transmit(&hi2c1, slave_addr, &fast_cmd, 1, 200);
//checks if there is a NACK, bus error, etc and turns led ON
if (status != HAL_OK) {
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_13, GPIO_PIN_SET);
} else {
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_13, GPIO_PIN_RESET);
}
HAL_Delay(5000); // Wait 5 seconds
//send address byte, wait for acknowledge from slave, send 1 data byte
status = HAL_I2C_Master_Transmit(&hi2c1, slave_addr, &slow_cmd, 1, 200);
//checks if there is a NACK, bus error, etc and turns led ON
if (status != HAL_OK) {
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_13, GPIO_PIN_SET);
} else {
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_13, GPIO_PIN_RESET);
}
HAL_Delay(5000); // Wait 5 seconds
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
Slave:
- Listening to the I2C in main using: HAL_I2C_EnableListen_IT(&hi2c1);
- changing the blink speed according to the data sent (1's/0's)
I2C_HandleTypeDef hi2c1;
uint8_t rx_buffer = 0; // Buffer to receive I2C data
volatile uint32_t blink_speed = 50; // Initial blink speed (ms)
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_I2C1_Init();
/* Enable I2C slave listening */
HAL_I2C_EnableListen_IT(&hi2c1);
while (1)
{
HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_13);
HAL_Delay(blink_speed);
}
}
void HAL_I2C_AddrCallback(I2C_HandleTypeDef *hi2c, uint8_t TransferDirection, uint16_t AddrMatchCode)
{
if (hi2c->Instance == I2C1 &&
TransferDirection == I2C_DIRECTION_TRANSMIT)
{
HAL_I2C_Slave_Receive_IT(hi2c, &rx_buffer, 1);
}
}
void HAL_I2C_SlaveRxCpltCallback(I2C_HandleTypeDef *hi2c)
{
if (rx_buffer == 0xFF)
{
blink_speed = 100;
}
else if (rx_buffer == 0x00)
{
blink_speed = 1000;
}
HAL_I2C_EnableListen_IT(hi2c);
}
void HAL_I2C_ListenCpltCallback(I2C_HandleTypeDef *hi2c)
{
HAL_I2C_EnableListen_IT(hi2c);
}
Edited to apply source code formatting - please see How to insert source code for future reference.