Skip to main content
AVain.1
Associate
May 24, 2020
Question

What can possibly cause USBLC6-2P6 failure?

  • May 24, 2020
  • 1 reply
  • 946 views

In our application USBLC6-2P6 is connected between a USB port and a processor STM32L4R5xx. The circuit is self-powered (Li-ion battery), and uses either PC USB or USB dc power supply for charging and communication. We find a number of damaged USBLC6-2P6 with a specific failure pattern: both low side diodes show 0.8V voltage drop in both direction, while both high-side diodes and a Vbus TVS diode are open (see image below). What can possibly cause these failures? Are there any test reports for this device and what are the typical failure modes?

This topic has been closed for replies.

1 reply

TKara.1
Visitor II
November 4, 2021

Has anyone from ST ever responded to you about this?