Skip to main content
PLang.2
Associate
February 12, 2020
Solved

What is the thermal resistance (junction to ambient) for the M24C32?

  • February 12, 2020
  • 2 replies
  • 1022 views

No detail about it in the datasheet. This is quite an old part design. I'm looking for the thermal resistance of the industrial version of the part (-40 to 85°C). I'm quite sure that the self-heating is minimum. But, I want characterization data that proves that it is.

This topic has been closed for replies.
Best answer by Pierre P.

​Hello,

The Value of 'Theta JA' (thermal resistance of junction to air) depends of the package of the EEPROM :

- SO8N (150 mils) : 219°C/W

- TSSOP8: 255°C/W

- MLP 2x3: 67°C/W

- WLCSP : < 40°C/W

BR

Team EEPROM suPPort 

2 replies

Pierre P.
Pierre P.Best answer
ST Employee
February 13, 2020

​Hello,

The Value of 'Theta JA' (thermal resistance of junction to air) depends of the package of the EEPROM :

- SO8N (150 mils) : 219°C/W

- TSSOP8: 255°C/W

- MLP 2x3: 67°C/W

- WLCSP : < 40°C/W

BR

Team EEPROM suPPort 

PLang.2
PLang.2Author
Associate
February 13, 2020

Thanks a lot for the answer.