Associate
March 13, 2023
Question
Why did my LoRaWAN app only sends empty data?
- March 13, 2023
- 0 replies
- 1407 views
I'm trying to send some GNSS data using LoRaWAN, but my gateway only receives a blank string. Pretty sure the AppData.Buffer values are right since it prints the right thing on my console.
As you can see my gateway didn't receive any payload.
Here's my SendTxData part
ReceiveGNSSData();
hdop = (uint8_t)(GNSSParser_Data.gpgga_data.acc * 10);
hour = (uint8_t)(GNSSParser_Data.gpgga_data.utc.hh);
minute = (uint8_t)(GNSSParser_Data.gpgga_data.utc.mm);
second = (uint8_t)(GNSSParser_Data.gpgga_data.utc.ss);
sats = (uint8_t)(GNSSParser_Data.gpgga_data.sats);
altitude = (int16_t)(GNSSParser_Data.gpgga_data.xyz.alt * 10);
AppData.Buffer[i++] = AppLedStateOn;
AppData.Buffer[i++] = (uint8_t)(hour & 0xFF);
AppData.Buffer[i++] = (uint8_t)(minute & 0xFF);
AppData.Buffer[i++] = (uint8_t)(second & 0xFF);
AppData.Buffer[i++] = (uint8_t)(sats & 0xFF);
// AppData.Buffer[i++] = (uint8_t)((altitude >> 16) & 0xFF); ga perlu soalnya datanya cuma 16 bit jadi cukup shift 8
AppData.Buffer[i++] = (uint8_t)((altitude >> 8) & 0xFF);
AppData.Buffer[i++] = (uint8_t)(altitude & 0xFF);
AppData.BufferSize = i;
APP_LOG(TS_OFF, VLEVEL_L,
"Send on port LORAWAN_USER_APP_PORT (%d): \r\n"
"Led : %s\r\n"
"UTC : %d:%d:%d\r\n"
"Sats : %d\r\n"
"Alt : %d.%d m\r\n",
LORAWAN_USER_APP_PORT,
AppData.Buffer[0] == SET ? "ON" : "OFF", // Led state
AppData.Buffer[1], AppData.Buffer[2], AppData.Buffer[3], // UTC
AppData.Buffer[4], // Satellites
(AppData.Buffer[5] << 8 | AppData.Buffer[6]) / 10, // Altitude 1
(AppData.Buffer[5] << 8 | AppData.Buffer[6]) % 10); // Altitude 2I also attached the full lora_app if needed. Thank you.