Skip to main content
Associate II
February 7, 2026
Solved

Why Does APM32F103 Timing Break After Standby Wake-Up on Identical Boards?

  • February 7, 2026
  • 2 replies
  • 323 views

Title edited to correct part number: it is a Geehy APM32F103CBT6 - not an STM32.

See this post.


Hi everyone,

I am working on a project using the STM32F103CB MCU and implementing Standby (low-power) mode in the firmware. Development is done using Arduino IDE v2.3.2. I want the standby mode to be implemented to reduce the current consumption since my device is battery-operated. 

Problem Overview

The firmware flow is as follows:

  • On power-up, setup() runs.

  • In loop(), if the reset reason is a power-on reset, the device enters Standby mode.

  • The MCU wakes up from Standby via an interrupt on PA0 (Wakeup Pin).

  • Execution flow and timing are monitored using the Serial Monitor.

With the same firmware and library versions, I am observing different behaviour on two PCBs that:

  • Have identical schematics

  • Are manufactured by the same vendor

Observed Behavior

  • Without Standby mode implemented, both PCBs behave correctly.

  • With Standby mode enabled:

    • Serial prints before entering Standby appear correctly.

    • After waking from Standby:

      • One PCB works as expected.

      • The other PCB shows:

        • Garbage characters in the Serial Monitor

        • Significantly extended timing

          • Example: a programmed delay(30 seconds) takes approximately 1 minute 10 seconds

          • All timing sources (delay(), millis(), etc.) appear slowed down

Clock Configuration

  • No external crystal or clock source is used.

  • The project relies only on the internal clock (HSI).

  • Clock information (SystemCoreClock, RCC registers) is printed after reset.

    • Problematic PCB - Shanmugapriya_1-1770482971129.png
    • Proper PCB - Shanmugapriya_0-1770482956593.png
  • From the serial output:

    • Clocks appear correct after a power-cycle reset

    • Clocks appear to be incorrect or degraded after waking from Standby on the problematic PCB

 

Test Code

I am attaching the test code used to reproduce the issue (shown below for reference):

 

#include <Arduino.h>
 
// ---------------- Pins ----------------
#define USB_PWR   PB0      // not used in this scenario, keep if needed
#define PWR_LED   PB1      // LED output (active HIGH)

// ---------------- Serial ----------------
HardwareSerial Serial1(PA10, PA9);   // rx, tx (STM32duino constructor = RX,TX)
#define pc Serial1

// ---------------- Timing ----------------
#define LED_ON_MS   15000UL   // 15 seconds

// ---------------- State ----------------
enum State : uint8_t { STATE_15S_ON_THEN_STBY, STATE_LED_ON_FOREVER };
static State state = STATE_15S_ON_THEN_STBY;

static uint32_t t_start = 0;

// ---- Helper: Enter Standby (never returns) ----
static void enterStandby()
{
  __HAL_RCC_PWR_CLK_ENABLE();
 
  // Make sure LED is off just before entering standby
  digitalWrite(PWR_LED, LOW);

  // Quiet the UART so we don't send while clocks change
  pc.flush();
  delay(2);
  pc.end();
  delay(5);

  // Required RM0008 sequence: disable, clear, then enable wakeup pin
  HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1);
  __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);   // clear any spurious wake
  // (Optional) clear StandBy flag so next boot can differentiate cleanly
  __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
  HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1); // PA0, rising edge

  // Enter Standby (resets on wake)
  HAL_PWR_EnterSTANDBYMode();

  // Should never get here
  while (1) { }
}

// ---- Helper: check if we woke from Standby ----
static bool wokeFromStandby()
{
  __HAL_RCC_PWR_CLK_ENABLE();
  return (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET);
}

void setup()
{
  // Detect boot reason *before* changing flags
  const bool from_standby = wokeFromStandby();

  // Clear flags early so next entry works as expected
  __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
  __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);

  // Bring up Serial a moment after reset for stable clocks
  delay(10);
  pc.begin(9600);
  delay(10);
 
  // Optional: confirm clocks
  pc.print("SystemCoreClock="); pc.println(SystemCoreClock);
  uint32_t cr = RCC->CR;
  pc.print("RCC->CR=0x"); pc.println(cr, HEX);
  pc.print("HSIRDY="); pc.println((cr & RCC_CR_HSIRDY) ? "1":"0");
  // If you ever use PLL from HSI:
  pc.print("PLLRDY="); pc.println((cr & RCC_CR_PLLRDY) ? "1":"0");

  // GPIO
  pinMode(PWR_LED, OUTPUT);
  digitalWrite(PWR_LED, LOW);    // start OFF

  pc.println();
  pc.println("=== Boot ===");
  pc.println(from_standby ? "Boot reason: wake from STANDBY" : "Boot reason: cold/power-on or other reset");

  if (from_standby)
  {
    // Requirement: after waking from standby, keep LED ON continuously
    digitalWrite(PWR_LED, HIGH);
    state = STATE_LED_ON_FOREVER;
    pc.println("Action: LED -> ON (continuous)");
  }
  else
  {
    // Cold boot: LED ON 15s, then go to standby
    digitalWrite(PWR_LED, HIGH);
    t_start = millis();
    state = STATE_15S_ON_THEN_STBY;
    pc.print("Action: LED -> ON (timed ");
    pc.print(LED_ON_MS);
    pc.println(" ms), then standby");
  }
}
 
void loop()
{
  if (state == STATE_LED_ON_FOREVER)
  {
    // Nothing else to do; stay awake and keep LED ON
    delay(1000);
    return;
  }

  // 15-second timed state then enter standby
  if ((millis() - t_start) >= LED_ON_MS)
  {
    pc.println("15 s elapsed -> LED OFF then enter STANDBY");
    delay(5);
    enterStandby();  // never returns
  }

  // Optional heartbeat for visibility
  static uint32_t lastPrint = 0;
  uint32_t now = millis();
  if (now - lastPrint >= 1000UL)
  {
    lastPrint = now;
    pc.print("[RUN] elapsed(ms)=");
    pc.println(now - t_start);
  }
}
 

Test Results

  • Case 1 – Problematic PCB

    • Serial output contains garbage after Standby wake-up

    • All timing functions run slower than expected

Shanmugapriya_0-1770482811321.png

  • Case 2 – Proper PCB

    • Serial output and timing behave correctly

Shanmugapriya_1-1770482839167.png

I have also included schematic diagrams for the power and controller circuits

Shanmugapriya_2-1770483300040.png    Shanmugapriya_3-1770483305630.pngShanmugapriya_4-1770483317801.png

 

Question

Why would two PCBs with the same schematic and firmware exhibit different clock behavior after exiting Standby mode, leading to timing issues on one board?

What could cause the system clock to collapse or run slower after Standby on only one PCB, and how can this be fixed?

Please let me know if additional information, measurements, or logs are required from my side.

Thanks in advance for your help.

Best answer by Peter BENSCH

Yes. Please contact the manufacturer Geehy for assistance.

2 replies

Peter BENSCH
Technical Moderator
February 7, 2026

Which STM32F103 are you really talking about?

In your last posts and now you mentioned the STM32F103CB, but in the schematics you have a STM32F103C8T6. If it really is the STM32F103C8T6, I suggest you first check whether it is an original – the STM32F103C8T6 is counterfeited in large quantities in Asia, sometimes with fake labelling to make it look like the original product.

There have been numerous posts on this topic in the community for years. Suitable search terms are "Blue Pill" or "Bluepill", "STM32F103C8T6", "fake" or "counterfeit".

If you have been duped by a counterfeit, you should either contact the counterfeiter or purchase an original device from an authorised dealer – Alibaba and similar sites are not authorised ones.

Regards
/Peter

Associate II
February 9, 2026

Thank you, Peter. 

I am using the APM32F103CBT6 MCU. Does this counterfeit issue apply to this MCU as well?
Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
February 9, 2026

Yes. Please contact the manufacturer Geehy for assistance.

Andrew Neil
Super User
February 9, 2026

@Shanmugapriya wrote:

Development is done using Arduino IDE v2.3.2..


Note that this forum concentrates on "conventional" development; for Aurduino issues, you'd be better at https://www.stm32duino.com/

Or the main Arduino forums: https://forum.arduino.cc/ 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.