Skip to main content
EJian.2
Associate II
October 26, 2022
Question

Why there is an inconsistent bewteen the label information and the marking information?

  • October 26, 2022
  • 1 reply
  • 1411 views

Why there is an inconsistent bewteen the label information and the marking information?We find the marking should be ,Judging from the label, its marking should be "STR712FR2", but actually its marking on the device is "ST712FR2".Why? If this is normal?0693W00000VO8ZQQA1.png

This topic has been closed for replies.

1 reply

Peter BENSCH
Technical Moderator
November 1, 2022

The STR712FR2 has long been discontinued, but there were several variants of the STR712FR2T6, including one with suffix $U5. This suffix has no technical relevance and is only used internally.

It is correct, however, that the laser marking on the $U5 variant was ST712FR2, on other variants also STR712FR2. Since these parts have long been discontinued, it is unfortunately no longer possible to determine why a different marking is printed on the label.

Does it answer your question?

Regards

/Peter

P.S.: it's not a legacy MCU anymore but a discuntinued one, so I changed the topic to "Discontinued Products".

Piranha
Principal III
November 1, 2022

The only tag is still "Legacy MCUs". And those are tags regardless of how FailForce mixes up names for obvious things...

Peter BENSCH
Technical Moderator
November 1, 2022

@Piranha​ even if this is a bit off-topic: when starting a question with "Post To", you can very well choose in which section it should appear:

  • ...
  • EEPROM
  • Legacy MCUs
  • ST Power Studio
  • Switches and Multiplexers
  • Discontinued Products

 

If you think that names are being mixed up, you are welcome to ask your own question about this.