Skip to main content
DZhou.1
Associate
February 3, 2020
Question

X-NUCLEO-GNSS1A1 expansion board wrong GPS location

  • February 3, 2020
  • 1 reply
  • 717 views

Hi,

I have two X-NUCLEO-GNSS1A1 expansion boards.

I powered on the first board, and connected to UART port. I can read GPS messages from the board. GPS location is good. (I got GPRMC and GPGGA, GPGLL, etc.) I don't know what I did. Somehow NMEA messages report zero gps locations (0.0 N, 0.0 E). the UTC time stamp seems good.

Then I replaced with the second board, it reports GPS position (somewhere in Italy). It shall report as in New York.

Is it required to setup or configure the GPS micro firmware? Or it needs to select which satellite to use? No clue. Hope someone can help.

Thank you,

David

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    February 3, 2020

    Should work out of the box.

    Make sure you can measure a DC bias on the RF feed as this will be needed to power the antenna. Put the antenna outside, with a clear view of the sky.

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..