ADP5091 using TEG
Hello,
I would like to use the converter SPV1050 in a new product of my company but I have some doubts. First of all, the application I need is to feed a harvesting device, which includes a supercapacitor of 5F and 5V. So, I need an output from the SPV1050 to feed my electronic device, let's say I just need a positive pin and negative pin with an output of 5V. Where I should connect the positive pin of my electronic? In BAT or STORE pin?
Another question is how I can configure the output to 5V.
If you could tell me the configuration I need to perform if I use the STEVAL-ISV019V1I would be very gratefull.
Thank you.