Skip to main content
STLearner
Associate III
April 24, 2023
Question

Battery charger solution

  • April 24, 2023
  • 1 reply
  • 786 views

Hi ST experts,

Would like to know if ST has any recommendation on battery charging solution?

The battery pack requirement is 7.4V 2300mAH which is 2-cells construction.

The intention is to change from standalone battery charger IC to a smart charger solution whereby it can help to prolong the battery lifespan for example having trickle charging and battery health (SOC) to keep the battery charge to max 80% (this can be done by configurable through software or hardware) and depth of discharge to 50% or 25%

Appreciate with any suggestions which can meets above-mentioned requirements.

Thanks.

    This topic has been closed for replies.

    1 reply

    Winfred LU
    ST Employee
    April 25, 2023

    Sorry. There is no solution fitting the requirements.

    Battery charger portfolio:

    https://www.st.com/en/power-management/battery-chargers.html