BTA26-80BWRG
Hello,
I have questions about a project we developed a long time ago. I will put the schematic below. We are using the BTA26-800BWRG (U8 and U9) in the schematic to parallel two inductors. The voltage applied to these two inductors is an ultrasonic signal of 600V at a frequency of 20-120 kHz. However, I don't fully understand how the TRIACs can switch, given that there is no voltage source in the loop between the two gates. Yet, the project works almost perfectly, except that sometimes, when the generator is off and the attempt is made to turn off the TRIACs, they remain switched on.

U8 & U9 (BTA26-800BWRG) & OP1 & OP2 (IL410)
Thank's in advance for your help.
Best regards,
Joe