Cannot connect STWBC86 to WPSTUDIO V1.8.4
Hi there,
we are trying to operate a STWBC86 on a rebuild of STDES-WBC86WTX.Eval boards are not yet available so we needed to build them with the given data on our own.
when powering it up nothing happens so i assumed i need to program the supplied Firmware onto it via WPSTUDIO.
When i try to connect to the board i get a Error message:

Wrong config ID and Patch Id for TX.
I even cannot use the programming section of the tool as the buttons are greyed out:

Documentation is very thin and doesnt`give information how to program the device on another way.
How do i proceed ? can anybody help me on that issue?
Best regards
Stefan
P.S: Hi there,
i was able to solve the issue by myself. You need to set the device to WBC86 and then Type to Empty to be able to program the device. afterwards everything works as intended.