Skip to main content
sabaRamin
Associate
August 20, 2022
Question

Driving LED1 signal on STPM32(electric meter ic) by STM32F1x

  • August 20, 2022
  • 0 replies
  • 664 views

Hi guys,

I connected STPM32 evaluation board (UART mode) to STM32F103 board.

I use of stpm32 firmware from st.com. and it work. I can measure and read rms voltage, rms current, active energy and.... . but when i set pulse/kwh LED on stpm32, I have below signal:

0693W00000QO86EQAT.jpgit is not a clear signal. it has a 50 hz on it too. why?

is it normal? or i must have only 0.721 Hz without 50Hz burst?

thank you

This topic has been closed for replies.