Skip to main content
Visitor II
July 18, 2024
Question

dynamic resistance of TVS

  • July 18, 2024
  • 1 reply
  • 648 views

Dear Sirs,

Could you advise me dynamic resistance(Rd) of TVS such as SM6T33CAY used to clamp against pulse 5B per ISO 7637-2 or load dump B in ISO 16750-2.load dump B_1.JPG 

Its voltage source waveform is clamped instead of exponential surge curve.

Thanks

John 

1 reply

Peter BENSCH
Technical Moderator
July 29, 2024

Welcome @JMan, to the community!

The question should be answered as you have already connected with your local contact so this thread can be closed?

Regards
/Peter