Skip to main content
Associate
November 13, 2024
Solved

E-L9823 pin 21 - NC

  • November 13, 2024
  • 1 reply
  • 675 views

Hi. Looking to use E-L9823 as a replacement in a legacy design.

The datasheet states pin 21 is not connected. Looking to confirm it is a true "no connect" internally on the part.  On our existing PCB it will be tied to +24V. Thanks.

Best answer by dcflipflop

I opened a case and received the following reply from ST Customer Support.  I have not tried the part in circuit yet.

"For N.C. Pins, there is absolutely no connection from the pin labeled NC to the die. So it is floating."

1 reply

Associate
February 11, 2025

Hello ,

Did you find solution?  I'm also dealing with the same issue.

dcflipflopAuthorBest answer
Associate
February 11, 2025

I opened a case and received the following reply from ST Customer Support.  I have not tried the part in circuit yet.

"For N.C. Pins, there is absolutely no connection from the pin labeled NC to the die. So it is floating."

Associate
February 12, 2025

Ok for my case, they connected it to 24V, still now no issues observed.