Skip to main content
Associate
September 26, 2025
Solved

ECMF4-20A42N10 vs ECMF04-4HSWM10

  • September 26, 2025
  • 1 reply
  • 477 views

Hello,

 

Please confirm if ECMF04-4HSWM10 is possible replacement for ECMF4-20A42N10?  ECMF4-20A42N10 is in LTB status and we need replacement part with "recommended for new design" status.

Thanks,

Quynh

Best answer by Peter BENSCH

Welcome @qnguyen, to the community!

You can consider the ECMF04-4HSWM10 as a possible replacement for the ECMF4-20A42N10, but it is neither a drop-in replacement (shorter package with a pitch of 0.4mm instead of the previous 0.5mm), nor are the technical data (e.g. frequency-dependent attenuation) absolutely identical.

Hope that helps?

Regards
/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
September 29, 2025

Welcome @qnguyen, to the community!

You can consider the ECMF04-4HSWM10 as a possible replacement for the ECMF4-20A42N10, but it is neither a drop-in replacement (shorter package with a pitch of 0.4mm instead of the previous 0.5mm), nor are the technical data (e.g. frequency-dependent attenuation) absolutely identical.

Hope that helps?

Regards
/Peter

qnguyenAuthor
Associate
September 29, 2025

Thanks Peter.

 

Quynh