Error Flashing firmware to STWLC98
Hello,
I have developed my own evaluation Board for the STWLC98 Chip. When connecting the power suplly, the DC-Mode, which is on the IC when it is delivered, works in a correct way. But when I want to program the IC with the following firmware from the ST Website:
STEVAL-WLC98RX_config_2C00.memh
STEVAL-WLC98RX_nvmpatch_1454.memh
I get the following errors, when the programming status bar reaches 100%:
Config Id Mismatch! file/chip: 0x2C00/0x1000
Wrong config id 0x1000 and patch id 0x0000 for RX
Where can I find the right Firmware or do you have any solutions for me?
Thank You
Simon