Skip to main content
bmose.1
Visitor II
February 16, 2021
Question

for phase cutting control we would like use either BTA16 (T0-220AB) or T1635 (D2PAK) on ouer PCB.the controlsignal is a 3,3 VDC pwm. ( see attachment ) A T1635H-6T is placed instead the T1635 in the boom list by a mistake .

  • February 16, 2021
  • 0 replies
  • 588 views

now we have following situation.

  1. the circuit works fine at using the BTA16
  2. at using the T1635H-6T the hase cutting doesn't works ( full wave is engaged over the PWM range )

Questions:

a. what is the difference between T1635 and T1635H-6T ?

b.how can we solved this problem ?

This topic has been closed for replies.