Skip to main content
Associate II
September 29, 2025
Question

GUI for tuning coil connected to STWLC38

  • September 29, 2025
  • 1 reply
  • 344 views

There are already a few posts which show there is an issue with getting the STSW-WPSTUDIO GUI downloaded. I replied to one, but I have yet to receive a response. I am looking to select capacitors to tune an RX coil connected to a STWLC38JR controller. It appears we need the GUI to accomplish this..?? Thanks in advance.

1 reply

Didier HERROUIN
Technical Moderator
October 16, 2025

Dera BPolinske,

The GUI is not needed to select the capacitors in series with the coil.
You should target a resonant frequency F=1/(2*P*√LC) = 90kHz based on your coil inductance (L).

For reference, in our STWLC38 eval kit, the coil is 8µH and the total capacitors are 400nF (4*100nF).

Best regards,

Didier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.