How to perform High-side switching of N-channel IGBT (STGW20NC60VD) if required gate-voltage is greater than the rated max gate voltage?
I am building an PV module I-V tracer that makes use of a capacitive load. In order to trace/record the current and voltage characteristics of the solar panel I am measuring the voltage and current that develops over the capacitive load as it charges from 0V to the open-circuit voltage(Voc) condition of the PV module. I am using a switching scheme to achieve this charging and discharging of the capacitive load using the STGW20NC60VD. The first switch is turned on to connect the PV module to the capacitive load. This connection is maintained until the capacitor charges to Voc where it is then discharged through a resistor by closing switch 2.
I am having a problem with switch 1. The configuration for switch 1 is such that the capacitive load is connected to the emitter of the IGBT, the source is connected to the PV rail and the gate is used to switch it on an off. I am aware that for a high-side configuration like this, that a voltage greater than the gate-threshold voltage + the voltage over the capacitive load, is required at the gate to turn on the IGBT. This voltage however will need to be Vge(th)+Voc, roughly 53V, which is much greater than the allowable gate voltage (+-20V). I have been struggling to find an alternative igbt with a maximum allowable gate voltage that will allow this voltage.
Please can someone assist me with how I can perform switching for this functionality?