Skip to main content
Associate
April 4, 2025
Solved

HVLED007

  • April 4, 2025
  • 1 reply
  • 311 views
Hello, Good Morning Can i design SMPS using HVLED007 which should work on universal input and should provide 24v 2amp at its output it is PFC too. The most challenging part is to calculate and wind flyback transformer. I've some transformer bobbins and cores with me but dont have complete data i have calculated data manually like MPL,AE etc. but still some data is unknown like core material. Is there any SMPS application note for this.
    Best answer by Peter BENSCH

    Welcome @D_N, to the community!

    The calculation of the corresponding transformer goes far beyond the data sheet of the HVLED007, which is why the AN1059 is mentioned there as a reference. There is a lot more information about transformer calculation, e.g. this presentation about Transformer Design Considerations from Wuerth Elektronik. Otherwise, the transformer manufacturer is usually very happy to help you select the right core.

    Hope that helps?

    Regards
    /Peter

    1 reply

    Peter BENSCH
    Peter BENSCHBest answer
    Technical Moderator
    April 4, 2025

    Welcome @D_N, to the community!

    The calculation of the corresponding transformer goes far beyond the data sheet of the HVLED007, which is why the AN1059 is mentioned there as a reference. There is a lot more information about transformer calculation, e.g. this presentation about Transformer Design Considerations from Wuerth Elektronik. Otherwise, the transformer manufacturer is usually very happy to help you select the right core.

    Hope that helps?

    Regards
    /Peter