Skip to main content
M.Graziani
Associate
March 29, 2023
Question

I would like to know if the component BTW691200 compared to the original is to be considered STM. The font and logo are very different. Thanks to all those will help me.

  • March 29, 2023
  • 3 replies
  • 1299 views

0693W00000aPNPhQAO.jpg0693W00000aPNPNQA4.jpg

    This topic has been closed for replies.

    3 replies

    Peter BENSCH
    Technical Moderator
    March 29, 2023

    Welcome, @M.Graziani​, to the community!

    It is difficult to tell from the photos.

    In order to be able to check this for sure, the Bulk ID from the label of the packaging is necessary, whose clearly legible photo should not be uploaded here in the public community, but by personal message.

    Regards

    /Peter

    Peter BENSCH
    Technical Moderator
    March 30, 2023

    We had already discussed the topic via PM, where I came to the conclusion that the component on the right side is almost certainly a fake.

    For the sake of comparison for others seeking advice, I am attaching an example picture from a Vietnamese dealer that does look a tiny bit like the thyristor in question - please compare for yourself. Chinese dealers, on the other hand, delete the fake logo from exactly the same picture:

    0693W00000bhECKQA2.jpg0693W00000bhECPQA2.jpg

    M.Graziani
    Associate
    March 31, 2023

    I have a last question...

    In the front of the component, where are the characters, there is a circle in the mold with an initials.

    What does it mean and if it is essential to recognize original and non-reprinted components?

    Thanks.

    Marco.

    Peter BENSCH
    Technical Moderator
    March 31, 2023

    This is the remnant from the ejector that remains after molding, where there should really be nothing but a smooth surface. If necessary, this can also be used to distinguish them from fakes.

    Regards

    /Peter

    Peter BENSCH
    Technical Moderator
    March 30, 2023

    If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

    Regards

    /Peter

    Tesla DeLorean
    Guru
    March 30, 2023

    @Peter BENSCH​ I do however remember seeing a PCN or Reliability report related to a change in the metal stamping/form when production was moved

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    Peter BENSCH
    Technical Moderator
    March 30, 2023

    @Community member​ Thanks for the tip. I have just looked through all the PCNs for the BTW69-1200 and found no reference to a change in the metal stamping/form. It is also noticeable that all the BTW69-1200 in question do not have the Eco character "G", and that the date code of the Asian variants has four digits (normal = three digits).