Skip to main content
Ritul Shah
Associate II
March 14, 2022
Question

Instant High Torque Application using STSPIN32F0

  • March 14, 2022
  • 2 replies
  • 909 views

Hello Madam/Sir,

@Cristiana SCARAMEL​ 

We are developing a PMSM motor drive for an industrial application. This application is for Sugarcane Juice machine where we require to provide instant high torque for a shorter duration.

I have developed a PMSM drive using the STSPIN32F0 controller. Drive is able to provide some 14 Amp loading for a small or a medium sized sugarcane on the motor instantly. But incase of a thicker sugarcane it may be requiring more Amps. But at that time, controller speed reduces significantly and gives a Speed Feedback or OverCurrent faults.

Motor parameters: 

Pole Pairs: 2

Nominal Voltage: 36V

Max Current: 25A

Nominal Speed: 1400 RPM

Rs: 0.48 Ohms

Ls: 2.5 mHenry

Bemf Constant: 17 KRPM/Vrms

Control Technique: 3 Shunt Sensorless FOC

I have few questions in which I require your guidance.

  1. Does this controller STSPIN32F0 support this power rating? (Approx 900 Watt) 
  2. Should I run the motor in Torque Control Mode or Speed Control Mode?
  3. Do I need to use 2 different PI loops? one for starting and another for Running conditions?
  4. How do I tune the Motor for this instantaneous Torque application? Please share a guide document if it is possible?
  5. I am Sharing the STMCX file for your reference. Let me know if you require any more information for the same.

Awaiting your reply soon.

Thank you

Ritul Shah

This topic has been closed for replies.

2 replies

Ritul Shah
Associate II
March 22, 2022

Can someone reply on this query?

SpinKernel
Associate III
June 15, 2022

Disable over current ;) Or make it something your comfortable with.

You would want Torque since speed isn't exactly your concern.

The rest i'm still struggling with myself.