Issue with STSW-L9961BMS - NO Device Found
Hello,
I am conducting tests using the STEVAL-L99615C evaluation board. Despite following the L9961BMS Quick Start Guide and User Manual, I am encountering an issue with Demo 1. As shown in the attached picture, the message "No device found" continues to appear. Even when applying 20V to the B+ and B- terminals, the same issue persists.
I have ensured that the hardware jumper pin settings match those specified in the Quick Start Guide. However, I am concerned that the difference in versions might be causing the problem. The version of Demo 1 in the Quick Start Guide is 1.1.0 (July 21, 2023), while the version I am testing is 1.3.0 (December 1, 2023). Could the change in version be causing this issue?
Thank you for your assistance.