L7987 in LDO when VIN < VOUT programmed
Hi
I am working on an application with wide VIN from 6V-60V and the target VOUT is 15V 3A max.
When VIN > 16V, L7987 should fit my application. Problem is that when VIN drops below 16V, eDesignSuite reports an error so simulation is not possible.
It states on L7987's datasheet that in case the input voltage falls close or below the programmed output voltage, L7987 is able to work in LDO mode. Am I correct? See screen capture of the datasheet below.
When L7987 works in LDO mode, does it mean the chip is able maintain Fsw with duty cycle lift to 100%?
What is the max. current in LDO mode?
Look forward to any comment.
John