Skip to main content
alexjafari2005
Associate II
November 5, 2016
Question

L7987LTR only provides 0.5 A max current rather than 2 A.

  • November 5, 2016
  • 2 replies
  • 773 views
Posted on November 05, 2016 at 19:04

Hi

I would like to use L7987LTR in a few designs. The datasheet of the IC says its able to provide 2 A current however I can only measure 0.5 A. I have tested the schematics in 3 different layouts and layouts all seem to be good but all have the same behaviour. This makes me believe the problem is not in layout.

Moreover, I have tried a few differnet inductors (10uH) and diodes but I only measure 0.5 A output current. What am doing wrong? why does not the IC provide more current?

Thank you for you time in advance.

L2 = NR8040T100M (3.1A 2 mOhm Max ), LQH43PN100M26L, 744045100

D5 = NRVTS260ESFT1G (650mV @ 2A), B340B-13-F (500mV @ 3A)

Best regards,

-Alex

#dc-dc-conversion #l7987

2 replies

alexjafari2005
Associate II
November 13, 2016
AMens.1
Associate II
December 23, 2024

Change R34 to 39K.

edit: oeps...just saw it's a very old post :see_no_evil_monkey: