Skip to main content
Associate III
February 22, 2026
Solved

Low Noise 5V to 400–1000V Adjustable HV Supply (1–200µA) for Portable System

  • February 22, 2026
  • 2 replies
  • 180 views

Hi,

We are designing a compact, battery-powered system that requires a regulated high-voltage DC output with the following specifications:

• Input: 5V

• Output: Adjustable 400V to 1000V

• Load current: 1µA to 200µA

• Very low ripple and noise

• High efficiency and small form factor

The supply will be used as a bias source for sensitive detectors (e.g., APD/PMT-type devices), so output stability and low noise are critical. The output must remain stable across the specified load range.

I am currently considering a closed-loop flyback topology with post-filtering, but I am open to alternative architectures.

Could you please recommend:

• Suitable controller ICs from your portfolio?

• Relevant reference designs or evaluation boards?

• Design techniques for minimizing ripple and noise at these voltage levels?

Any guidance or application notes would be greatly appreciated.

Thank you.

 

 

Best answer by RobK1

This application note by the late, great Jim Williams might be of some interest to you:

AN118: High Voltage, Low Noise, DC/DC Converters A Kilovolt with 100 Microvolts of Noise | Analog Devices

2 replies

Peter BENSCH
Technical Moderator
February 23, 2026

In principle, this can be done with a flyback, but the effort required in relation to the output power is probably too great and a flyback would be significantly oversized. You should therefore consider something that has been used for many decades to generate high voltages with low output currents: a voltage multiplier, i.e. something similar to a Cockcroft-Walton generator. With 12..13 stages, you should achieve 1kV with some control reserve; 15...22nF capacitors should be sufficient.

Advantages:

  • Minimal system volume (no large, expensive and complex transformers are required)
  • Ripple and noise can be easily controlled with sufficiently high frequency and RC filters
  • Voltage can be regulated via the switching frequency (~100kHz...few MHz) and/or PWM

Disadvantages:

  • Sufficiently high voltage capacitors
  • Many high-voltage ultrafast diodes due to the necessary multiplier stages

You should urgently observe the usual precautions to minimise ripple and noise:

  • Layout with star-shaped GND, strictly separated from the signal grounds (reference voltage, opamp controller, etc)
  • Air and creepage distances sufficiently large and also as far away as possible from the signal paths

There are a few devices in the portfolio of STMicroelectronics that you can use in such a voltage multiplier:

Hope that helps?

Regards
/Peter

Zaim01Author
Associate III
February 25, 2026

Thanks Peter for the answer its helpful.

RobK1
RobK1Best answer
Associate II
February 24, 2026

This application note by the late, great Jim Williams might be of some interest to you:

AN118: High Voltage, Low Noise, DC/DC Converters A Kilovolt with 100 Microvolts of Noise | Analog Devices

Zaim01Author
Associate III
February 25, 2026

Thanks. this is exactly what i was looking for.