Manual rotation of the stepper motor shaft to start the PowerSTEP01 controller.
I wonder if it is possible without external sensors by manually rotating the stepper motor shaft to initiate the PowerSTEP01 controller. Manual rotation of the shaft triggers the controller while informing it of the motor's direction of operation. After this trigger, the specified sequence of work is executed after which the system goes into standby and waits for the next manual trigger of work.