PM8805 - Potential Damage to Active Bridge FETs
We are currently using the PM8805 in our PD (Powered Device) design.
We have recently encountered field failures and suspect that the root cause lies in the customer's testing process.
Our customer was using a Passive DC Injector (55V DC Supply) instead of a standard IEEE 802.3at/bt compliant PSE. During their inspection, they perform "Hot-plugging" of the 55V DC source directly into the RJ45 port.
I’m assuming the PM8805 has to 'work through' the Active Bridge’s body diodes during the initial handshake (Detection/Class). Since the MOSFETs aren't active yet, all that signaling current must be passing through the parasitic diodes, correct?
My concern is that when using a 55V direct injector, a massive amount of inrush current is forced through these body diodes before the voltage even reaches the UVLO threshold. Doesn't this put a lethal amount of stress on the bridge before the PM8805 can even start its control sequence?
We performed a failure analysis on the damaged products and found the body diodes in a dead-short state. This explains why we couldn't detect any Classification current—the 55V direct injection simply killed the bridge diodes before the PM8805 had a chance to perform its standard PoE sequence.
I would like to get your official confirmation on whether my hypothesis is correct. Also, if there are any other potential causes or failure mechanisms we should consider regarding this 'diode short' issue under these specific conditions, please let us know your professional insight.
I look forward to hearing from you. Thank you in advance.