Power good (PG) pin on LD39100
Hi
I am looking some guidance how to use the PG pin to indicate the power good mode with fixed versions of LD39100. (3.3 and 1.8V versions.) I plan to use the 3.3V output as an input for the fixed 1v8 ldo version, so ideally all I need to monitor to verify the functionality is the PG pin from 1.8V version of LDO.
PG pins I plan to pull-up high to Vin and datasheet suggest using a resistor between 100kOhm and 1Mohm. I assume that with the fixed 3.3V version of LD39100, the voltage should be high enough to power up the LED directly but with the 1.8V ldo case, I should use it more like an IO pin and then supply the LED voltage from LDO 3.3V?