Question
power source
- November 14, 2025
- 0 replies
- 152 views
Hello, (L6562DTR)I have encountered some problems when using this chip and hope to get some suggestions from you; ”The PF output voltage of 480V FC load is 0.7435“ The power input voltage is 250V-528VAC, with PFC+ flyback. The PFC BUS voltage is 760V, and the power output is 150W;When the input is 480VAC and the output is fully loaded, the THD is abnormal, ranging from 10% to 20% (5% for normal products), and at the same time, the PF value also drops and there is noise from the power supply
How can this problem be avoided