Skip to main content
Associate
June 28, 2024
Question

Question about the STEVAL-CTM009V1 board

  • June 28, 2024
  • 0 replies
  • 557 views

Hi Sir/Ma'am,

I have a question about the STEVAL-CTM009V1 board.

Explanation: Currently, I am using the STEVAL-CTM009V1 evaluation kit for my motor control application. I have connected the necessary power supplies(48V and 12V) and all 4 RED LEDs are ON. I applied 6 PWMs and tested that I could see the PWMs at the input of the gate driver and also there is a 3.3 V available at SD&OD pin. But I am not receiving any output other than small spikes at the low sides output and LOW at high sides output. 

Questions: what could be the possible reason behind this?