Skip to main content
Visitor II
January 9, 2024
Solved

RCD Snubber

  • January 9, 2024
  • 1 reply
  • 1675 views

I'm designing a automatic fan switch using a BTA26-800CWRG triac.  I'm planning on a RCD snubber.  All I've seen so far show a single diode across the resistor of the snubber.  But it seems if the snubber is snubbing an AC source there should be two parallel back to back diodes to handle both the positive and negative sources.  Can anyone confirm or shed some light on the subject?  Thanks.

This topic has been closed for replies.
Best answer by Peter BENSCH

Welcome @Rod, to the community!

Unfortunately, you have not given any sources where you have found such a structure with a diode. If a snubber is required (the BTA26-800CWRG is a so-called snubberless TRIAC), then it is normally inserted as an RC element (see e.g. AN437).

Regards
/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
January 10, 2024

Welcome @Rod, to the community!

Unfortunately, you have not given any sources where you have found such a structure with a diode. If a snubber is required (the BTA26-800CWRG is a so-called snubberless TRIAC), then it is normally inserted as an RC element (see e.g. AN437).

Regards
/Peter