Skip to main content
Visitor II
October 30, 2025
Solved

SCTWA70N120G2V Ron data

  • October 30, 2025
  • 1 reply
  • 139 views

I want the specific Ron data corresponding to different VGS values (e.g., 8V–15V) when the MOSFET switch SCTWA70N120G2V is in the linear region.

Best answer by Peter BENSCH

Welcome @Kyle4, to the community!

the SCTWA70N120G2V is manufactured using a technology, which, due to its structure, is targeted for switching applications. If this transistor is nevertheless operated in the linear region, there is a significant risk of hotspots forming in its drain structure, which will lead to avalanche-like destruction of the transistor.

For further and more detailed questions, I recommend contacting the FAE of the local distributor or sales office.

Good luck!

Regards
/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
October 30, 2025

Welcome @Kyle4, to the community!

the SCTWA70N120G2V is manufactured using a technology, which, due to its structure, is targeted for switching applications. If this transistor is nevertheless operated in the linear region, there is a significant risk of hotspots forming in its drain structure, which will lead to avalanche-like destruction of the transistor.

For further and more detailed questions, I recommend contacting the FAE of the local distributor or sales office.

Good luck!

Regards
/Peter