Spv1050 battery charging issue
I have made a custom pcb of STEVAL-ISV019V1 circuit. In that ,we need to charge 3.7v lithium ion battery via USB supply and solar panel. When I connect USB supply or panel voltage as input voltage the complete input voltage is coming in the battery charging point. where as the lithium battery can only be charged up to 4.2V.when I measure the open voltage at battery charging point it appears greater than 4.2V.How can we set the charging voltage and also how can I measure the open voltage at fully charged condition?