Solved
This topic has been closed for replies.
Welcome, @Oliver, to the community!
Correct, this is the Z0109SN in the SOT-223.
The letter S stands for VDRM=700V, which is rather uncommon at present (in the data sheet only M/N for 600/800V is listed).
However, you can easily replace it with a Z0109NN with 800V, but I would strongly advise against getting the 600V type Z0109MN!
Currently, the Z0109NN is available in two versions in the eStore as Z0109NN 5AA4 and Z0109NN6AA4, whereby the additional numbers 5AA4 and 6AA4 refer to the size of the tape&reel, so they are irrelevant for you in single-unit quantities - you can take either one.
Hope that helps?
Regards
/Peter
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.