STC3100 Current register nonsense values
Hi,
I am having the same issue as this previous forum post, but the question was never answered.
Voltage and temperature sense give expected readings.
REG_VOLTAGE_LOW: 29; REG_VOLTAGE_HIGH:6 --- VOLTAGE: 3818mV
REG_TEMPERATURE_LOW: 186; REG_TEMPERATURE_HIGH:0 --- TEMP: 23 deg
from the datasheet ---> current (mA) = current_code* 11.77 / Rsense (mΩ)
REG_CURRENT_LOW: 203; REG_CURRENT_HIGH: 54 --- CURRENT: 15429mV
Where the actual current for my application is 2.5A. I am using a 10mOhm current sense resistor. Indeed a multimeter reveals 25mV drop across it.
Could somebody please tell me if this is a hardware issue? I have followed all recommendations in the datasheet closely, but cannot find a reason that current is this high. Furthermore, when my application draws only 3.5mA, the current reads 18018mA
Thank you very much.